LPC546XX User Guide and CAN Bus Info.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC546XX User Guide and CAN Bus Info.

1,794件の閲覧回数
jays
Contributor II

Hello,

I'm using the LPC564xx User Manual UM10912 Rev 2.2 for some CAN info. Right now I'm trying to figure out the TX FIFO, queue and dedicated buffer relationship and have a problem with the documentation. To me it seems that sections 35.14.7.3 Tx FIFO and 35.14.7.4 Tx queue on page 756 aren't correct and some of the info in the Tx FIFO section is for the Tx queue.

35.14.7.3 Tx FIFO
Tx queue operation is configured by setting the TFQM bit in the TXBC register. Messages
stored in the Tx queue are transmitted starting with the message with the lowest message
ID (highest priority). In case multiple queue buffers are configured with the same message
ID, the queue buffer with the lowest buffer number is transmitted first.

35.14.7.4 Tx queue
Tx queue operation is configured by programming the TFQM bit field to a value of one.
Messages stored in the Tx queue are transmitted starting with the message with the
lowest message ID (highest priority). In case that multiple queue buffers are configured
with the same message ID, the queue buffer with the lowest buffer number is transmitted
first.

Is there an updated user manual or a better on line reference for the LP546XX CAN interface?

Thank you.

Jay S.

ラベル(2)
1 返信

1,553件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jay Schwichtenberg.

Thanks for your sharing, I have reported this to development team, they said will fix it next version.

BR

Alice

0 件の賞賛
返信