LPC54618 SPI Interrupt example code not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC54618 SPI Interrupt example code not work

跳至解决方案
3,057 次查看
chengyohuang
Contributor I

HI

I downloaded the SPI interrupt example code of SDK_2.2_LPCXpresso54618 to my LPC54618 CAN FD Kit and i did not make any changes code,but SPI slave always received error.I connects  to J14-1.2.3.4

pastedImage_1.png

and i read the spi interrupt "readme.txt" file,Is the example SPI Master PIN correct?because i connects  to J9-PIN10.11.12.13 have SPI Master Data(0~63).But connects  to J9-PIN9.11.13.15 have nothing

pastedImage_2.png

This is my way of connecting the entity

pastedImage_4.jpg

pastedImage_5.png

What can I do to make the SPI interrupt example code successful?@#

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
2,655 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Cheng yo huang,

   This code is working in revB, but LPCXpress54618 rev C need to take care JS34, JS35, you need to modify the board connect, you need solder it in the correct position.

pastedImage_1.png

Besides, you need to connect JP6.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,655 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Cheng yo huang,

   This code is working in revB, but LPCXpress54618 rev C need to take care JS34, JS35, you need to modify the board connect, you need solder it in the correct position.

pastedImage_1.png

Besides, you need to connect JP6.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,655 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Cheng yo huang,

   Please remove the CAN FD board, check the LPCXpresso 54618 board version, what the version you are using?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复