LPC54608 and Flash Magic

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54608 and Flash Magic

1,473 次查看
実奥山
Contributor II

I could program LPC54608 by Flash Magic(USART mode).

But it is free software.

Can I use flash magic for a programming of a product?

okuyama

标签 (1)
0 项奖励
回复
1 回复

1,363 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello 実 奥山,

Do you mean you want to program your product (based on LPC54608) ?

If yes, sure, you can .


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复