LPC54608 and Flash Magic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 and Flash Magic

1,486件の閲覧回数
実奥山
Contributor II

I could program LPC54608 by Flash Magic(USART mode).

But it is free software.

Can I use flash magic for a programming of a product?

okuyama

ラベル(1)
0 件の賞賛
返信
1 返信

1,376件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello 実 奥山,

Do you mean you want to program your product (based on LPC54608) ?

If yes, sure, you can .


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信