LPC54608 Xpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54608 Xpresso

14,004 Views
eli_hughes
Contributor V

Christmas came early for me this year!   I managed to get a hold of some of the new LPCXpresso54608 boards.

LPCXpresso54608-1.jpg

LPCXpresso54608.jpg

What caught my eye was the combination of a TFT,  external SDRAM,  audio codec and a digital MIC.   I had been looking for a good board to teach an audio processing course at PSU this Spring.   It seems that may have found it.  Last week at the Embedded Systems Conference I gave a technical session on utilizing the DSP instructions in the Cortex M4 and M7 cores.   Since I had this board, I decided to make my own audio badge:

badge.jpg

It was a quick demo of using the TFT with the DMIC and the ARM CMSIS DSP libraries.     You can see I am plotting the time domain and the magnitude of an FFT in real time.  It made for a very nice and fluid demonstration.     I will have a spectrogram mode as soon as I get a bit more time.   

LPC546xx family is looking pretty cool. I believe the LPCXpresso 54608 board will be out shortly for purchase through the common distributors. The new  I highly recommend getting your hands on one.   It is a nice board for playing around with the Cortex M4 core and doing some audio processing.   The board  also has Dual USB (a feature I like in the LPC43xx series), SD Card, Ethernet and 8 Megabytes of RAM.    Not a bad deal at all!

Labels (3)
Tags (4)
13 Replies

9,856 Views
altium2
Contributor II

Really cool

0 Kudos
Reply

9,856 Views
zhougong98
Fresh Out Contributor

think you!

0 Kudos
Reply

9,856 Views
zhouli
Contributor I

Very nice

0 Kudos
Reply

9,856 Views
zhougong98
Fresh Out Contributor

very good LPC54608 For my car project,I use LPC MCU serial From LPC1100  LPC1700 LPC800 ,Now New Project need the chip IC like LPC54608 For TFT_LCD GUI Display 

0 Kudos
Reply

9,856 Views
bjtdhj
Contributor I

喜欢........................

0 Kudos
Reply

9,856 Views
mr_ming
Contributor II

nice!

0 Kudos
Reply

9,856 Views
eli_hughes
Contributor V

9,856 Views
okcn
Contributor III

Is it possible to share your code ?

0 Kudos
Reply

9,856 Views
joezhou-mcu
Contributor III

Thanks for sharing! Merry Christmas!

0 Kudos
Reply

9,856 Views
z_
Contributor I

Lucky guy ! Christmas !

0 Kudos
Reply

9,856 Views
exson
Contributor II

Christmas

0 Kudos
Reply

9,856 Views
okcn
Contributor III

Lucky guy !      Christmas  !

0 Kudos
Reply

9,855 Views
brendonslade
NXP TechSupport
NXP TechSupport

Thanks for sharing Eli!

Any chance of a video of your spectrum analyzer? :-)