LPC54608 XTAL PCB layout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54608 XTAL PCB layout

1,872 次查看
実奥山
Contributor II

I'm planning to make 4 layer board of LPC54608.

The thickness is t1.6.

I attach the outline of athe board.

L1 is circuit  layer.

L2 is GND layer.

L3 is power layer.

L4  is circuit  layer.

I'm planning to empty L2,L3 under XTAL.

But I don't know how to do L4.

Should I put GND pattern  in L4?

Or should I empty L4?

Please instruct me.

标签 (1)
0 项奖励
回复
1 回复

1,755 次查看
soledad
NXP Employee
NXP Employee

Hi,

The first thing to consider it is your Stackup,  L2 GND and L3 Power it is a mistake, you should use   L1 Circuit, L2 Power L3 Circuit, L4 GND.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复