LPC54608 XTAL PCB layout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 XTAL PCB layout

1,823件の閲覧回数
実奥山
Contributor II

I'm planning to make 4 layer board of LPC54608.

The thickness is t1.6.

I attach the outline of athe board.

L1 is circuit  layer.

L2 is GND layer.

L3 is power layer.

L4  is circuit  layer.

I'm planning to empty L2,L3 under XTAL.

But I don't know how to do L4.

Should I put GND pattern  in L4?

Or should I empty L4?

Please instruct me.

ラベル(1)
0 件の賞賛
返信
1 返信

1,706件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The first thing to consider it is your Stackup,  L2 GND and L3 Power it is a mistake, you should use   L1 Circuit, L2 Power L3 Circuit, L4 GND.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信