LPC54606 Reinvoke UART ISP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54606 Reinvoke UART ISP

2,273件の閲覧回数
gph
Contributor III

Hi,

I'am trying to Reinvoke ISP UART0 from IAP with no success.

ECRP say ISP and IAP mode are authorized.

The function Reinvoke is called and doesn't return (no error).

But the ISP tested with FlashMagic doesn't respond.

The bootloader is called, because if i set the ISP0 pin to low level, it's Ok.

But my need is to go in ISP mode without open the box and put the pin to ground.

Why when calling IAP with ispmode=6 the UART doesn't work ?

Does anyone have any advice ?

Thanks, Philippe

 

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,255件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gph 

 

I highly recommend you refer to: 

https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-ReinvokeISP-on-LPC54618/m-p/1351500  

 

Please contact me if still have issue. Thank you.

 

BR

Alice

0 件の賞賛
返信

2,248件の閲覧回数
gph
Contributor III
Hello,
Thanks.

I see this one and other post on forum, but no way.
My problem seems it's the bootloader who doesn't start in UART mode ...
Even when i specify mode 6.
0 件の賞賛
返信

2,223件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gph 

 

Can UART PORT function properly with the ISP pin?

If yes, please  share your project  and  steps. I'd be glad to help you review them.

Thanks!

 

BR

Alice

0 件の賞賛
返信

2,152件の閲覧回数
gph
Contributor III

Hi,

Yes with ISP pin it's working well.

I can't post all project. But here after related things.

 

Electronic part :

gph_0-1747818098936.pnggph_0-1747818098936.png

 

Code part : 

function called after reset and initialisation who start ISP if tag present in eeprom.

static void ISPCheck(void)
{
	uint8_t isp[3]={'?','?','?'};
	uint32_t st=0;
	uint8_t ispmode=6U;

	if(E2P_I2C_Read(EP2_ISPADDRESS, isp, sizeof(isp))==kStatus_Success)
	{
		if(isp[0]=='I' && isp[1]=='S' && isp[2]=='P')
		{
			LED_J_Set(false);
			isp[0]='?';
			isp[1]='?';
			isp[2]='?';
			E2P_I2C_Write(EP2_ISPADDRESS, isp, sizeof(isp));
			//delayms(100);
			//CLI_DirectPrintLine("!!! MODE ISP !!!");
			USART_Deinit(FLEXCOMM0_PERIPHERAL);
			//delayms(100);
			//__disable_irq();
			GPIO_PinWrite(GPIO, 0, 4, 0);
			delayms(100);
		    IAP_ReinvokeISP(ispmode, &st);	// Ne retourne pas si OK
		    CLI_DirectPrintLine("ISP : Fail !");
		}
//		else
//			CLI_DirectPrintLine("ISP : No request");
	}
	else
		CLI_DirectPrintLine("ISP : Read Error");
}

 

 

 

0 件の賞賛
返信

2,146件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gph 

I reviewed the content you shared。

I recommend debugging the code step-by-step to check the value of the variable ispmode before calling IAP_ReinvokeISP(ispmode, &st).

Additionally, use logic analysis to measure the signals on UART0 TX/RX and verify their integrity.

I also suggest you testing the demo first via the link below:

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC54XXX-How-To-Use-USB-Port-To-Update-F... 

 

BR

Alice

0 件の賞賛
返信