LPC54605JXXXET180 Pin compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54605JXXXET180 Pin compatibility

ソリューションへジャンプ
1,784件の閲覧回数
guitardenver
Contributor IV

Hello,

 

I am using the LPC54605J256ET180 parts. I wanted to ask NXP to confirm that the LPC54605J512ET180 is a pin for pin compatible part and can be a drop in replacement. Is the only difference the increase in FLASH and RAM?

 

If you happen to know of any of the other LPC546XXJXXXET180 parts are drop in that will also save me a lot of time from going through each pin and peripheral to confirm.

 

Thanks,

Matt

0 件の賞賛
返信
1 解決策
1,775件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Matt

Yes, these two parts are pin to pin compatible. The only difference is FLASH/RAM size.

  Flash/kB SRAM/kB
LPC54605J256ET180 256 136
LPC54605J512ET180 512 200

 

Have a nice day,

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,776件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Matt

Yes, these two parts are pin to pin compatible. The only difference is FLASH/RAM size.

  Flash/kB SRAM/kB
LPC54605J256ET180 256 136
LPC54605J512ET180 512 200

 

Have a nice day,

Jun Zhang

0 件の賞賛
返信