LPC54605JXXXET180 Pin compatibility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC54605JXXXET180 Pin compatibility

跳至解决方案
1,816 次查看
guitardenver
Contributor IV

Hello,

 

I am using the LPC54605J256ET180 parts. I wanted to ask NXP to confirm that the LPC54605J512ET180 is a pin for pin compatible part and can be a drop in replacement. Is the only difference the increase in FLASH and RAM?

 

If you happen to know of any of the other LPC546XXJXXXET180 parts are drop in that will also save me a lot of time from going through each pin and peripheral to confirm.

 

Thanks,

Matt

0 项奖励
回复
1 解答
1,807 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Matt

Yes, these two parts are pin to pin compatible. The only difference is FLASH/RAM size.

  Flash/kB SRAM/kB
LPC54605J256ET180 256 136
LPC54605J512ET180 512 200

 

Have a nice day,

Jun Zhang

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,808 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Matt

Yes, these two parts are pin to pin compatible. The only difference is FLASH/RAM size.

  Flash/kB SRAM/kB
LPC54605J256ET180 256 136
LPC54605J512ET180 512 200

 

Have a nice day,

Jun Zhang

0 项奖励
回复