LPC54605JXXXET180 Pin compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54605JXXXET180 Pin compatibility

Jump to solution
1,833 Views
guitardenver
Contributor IV

Hello,

 

I am using the LPC54605J256ET180 parts. I wanted to ask NXP to confirm that the LPC54605J512ET180 is a pin for pin compatible part and can be a drop in replacement. Is the only difference the increase in FLASH and RAM?

 

If you happen to know of any of the other LPC546XXJXXXET180 parts are drop in that will also save me a lot of time from going through each pin and peripheral to confirm.

 

Thanks,

Matt

0 Kudos
Reply
1 Solution
1,824 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Matt

Yes, these two parts are pin to pin compatible. The only difference is FLASH/RAM size.

  Flash/kB SRAM/kB
LPC54605J256ET180 256 136
LPC54605J512ET180 512 200

 

Have a nice day,

Jun Zhang

View solution in original post

0 Kudos
Reply
1 Reply
1,825 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Matt

Yes, these two parts are pin to pin compatible. The only difference is FLASH/RAM size.

  Flash/kB SRAM/kB
LPC54605J256ET180 256 136
LPC54605J512ET180 512 200

 

Have a nice day,

Jun Zhang

0 Kudos
Reply