LPC54102 Deep sleep wake up on I2C slave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54102 Deep sleep wake up on I2C slave

2,287件の閲覧回数
genisaguilar
Contributor II

I'm using a LPCXpresso54102 board and I'm trying to enter DEEP_SLEEP mode and wake up by I2C slave interrupt. I've followed the instructions in the manual (UM108050, section 25.4.3.2) and done all the steps in the required order. Anyway, no matter what order I try, I don't manage to wake up on I2C.  Code works well if I don't sleep.

Any ides of what I'm doing wrong. See the code below:


#define MK_BRIDGE_I2C_PORT                LPC_I2C2
#define MK_BRIDGE_I2C_INTHAND             I2C2_IRQHandler
#define MK_BRIDGE_IRQNUM                  I2C2_IRQn
#define MK_BRIDGE_WAKEUP_SRC            SYSCON_STARTER_I2C2
#define MK_BRIDGE_I2C_SCL_PIN            27
#define MK_BRIDGE_I2C_SDA_PIN            28
#define MK_BRIDGE_I2C_SCL_FN            IOCON_FUNC1
#define MK_BRIDGE_I2C_SDA_FN            IOCON_FUNC1
#define MK_BRIDGE_I2C_SLVADD            0x29
#define MK_BRIDGE_I2C_CLK_DIVIDER         (2)
#define MK_BRIDGE_I2C_SPEED       NRF_TWI_FREQ_100K


int main(void)
{
    Board_Init();
    NVIC_EnableIRQ(MK_BRIDGE_IRQNUM);
    Chip_SYSCON_EnableWakeup(MK_BRIDGE_WAKEUP_SRC);

    /* Enable the I2C controller */
    Chip_I2C_Init(MK_BRIDGE_I2C_PORT);

   Chip_I2CS_Enable(MK_BRIDGE_I2C_PORT);


    /* Initialize I2C pins */
    Chip_IOCON_PinMuxSet(LPC_IOCON, MK_BRIDGE_I2C_SCL_PORT,
            MK_BRIDGE_I2C_SCL_PIN,
            (MK_BRIDGE_I2C_SCL_FN | IOCON_DIGITAL_EN));
    Chip_IOCON_PinMuxSet(LPC_IOCON,
            MK_BRIDGE_I2C_SDA_PORT,
            MK_BRIDGE_I2C_SDA_PIN, (MK_BRIDGE_I2C_SDA_FN | IOCON_DIGITAL_EN));

    /* Setup clock rate for I2C */ //JH: check if we need that
    Chip_I2C_SetClockDiv(MK_BRIDGE_I2C_PORT, MK_BRIDGE_I2C_CLK_DIVIDER);

    /* Slave address on index 0 */
    Chip_I2CS_SetSlaveAddr(MK_BRIDGE_I2C_PORT, 0, MK_BRIDGE_I2C_SLVADD);

    /* Clear interrupt status and enable slave interrupts */
    Chip_I2CS_ClearStatus(MK_BRIDGE_I2C_PORT, I2C_STAT_SLVDESEL);
    Chip_I2C_EnableInt(MK_BRIDGE_I2C_PORT, I2C_INTENSET_SLVPENDING | I2C_INTENSET_SLVDESEL);

    while(1) {
        for(int j = 0; j < 5; j ++) {
            for (int i = 0; i < 100000;i++);
            Board_LED_Set(1, 1);
            for (int i = 0; i < 100000;i++);
            Board_LED_Set(1, 0);
        }

        Chip_POWER_EnterPowerMode(
                POWER_DEEP_SLEEP,
                SYSCON_PDRUNCFG_PD_WDT_OSC |
                    SYSCON_PDRUNCFG_PD_SRAM0A |
                    SYSCON_PDRUNCFG_PD_SRAM0B |
                    SYSCON_PDRUNCFG_PD_SRAM1 |
                    SYSCON_PDRUNCFG_PD_SRAM2 |
                    SYSCON_PDRUNCFG_PD_32K_OSC|
                    SYSCON_PDRUNCFG_PD_BOD_RST|
                    SYSCON_PDRUNCFG_PD_BOD_INTR);
    }

}

ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,973件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Genis,

   Before you enter deep sleep mode, did you change the clock to use the internal IRC as the the main clock?

  Please check this information from the user manual:

pastedImage_1.png

Please check it at first.

Any updated information, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,973件の閲覧回数
genisaguilar
Contributor II

Thank you Kerry, that was it. After changing to IRC clock now LPC wakes up on I2C. Still, I noticed that the first packet after waking up was always lost, I don't exactly know the reason why. I added a pin interrupt that awakes the micro some milliseconds before the master sends the I2C address.

0 件の賞賛
返信

1,973件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Genis Aguilar,

   Thanks for your updated information.

   Please do the test in the I2C slave after it is waked up. After it is waked up, you can toggle the GPIO, just to check the MCU is really waked up. Then you can send some other I2C data to the slave.

   Besides, you said:the first packet after waking up was always lost.

  Do you mean the second packet has no problem?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,973件の閲覧回数
genisaguilar
Contributor II

Yes, that's it: first packet wakes up the microcontroller but is lost, whereas the second one is received correctly. That may be due to implementation details or some timing issues, I don't know. Anyway I could sort that out by connecting a new line from I2C master which wakes slave mcu a few milliseconds before the I2C address is sent. I have plenty of free pins so that's not a problem right now.

0 件の賞賛
返信