LPC54018 SPI EOT & EOF USE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54018 SPI EOT & EOF USE

1,290 次查看
Sukumar_M
Contributor I

Hi,

I have config SPI LPC54018 EVK when we use EOT & EOF please Describe me

0 项奖励
回复
1 回复

1,284 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sukumar,

Regarding the EOT and EOF, pls refer to section 27.7.3.2 Frame_delay and 27.7.3.3 Transfer_delay in UM11155.pdf.

The EOF setting means that SPI master will insert delay between each transmitting data, but the /CS remain LOW between two transfer, the Frame Delay time is defined in SPI Delay register.

The EOT setting means that SPI master will insert delay between each transmitting data, meanwhile the /CS is driven to HIGH between two transfer, the Transfer Delay time is defined in SPI Delay register. That the /CS is set high means that the transfer is completed.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复