LPC54018 SPI EOT & EOF USE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54018 SPI EOT & EOF USE

1,293件の閲覧回数
Sukumar_M
Contributor I

Hi,

I have config SPI LPC54018 EVK when we use EOT & EOF please Describe me

0 件の賞賛
返信
1 返信

1,287件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sukumar,

Regarding the EOT and EOF, pls refer to section 27.7.3.2 Frame_delay and 27.7.3.3 Transfer_delay in UM11155.pdf.

The EOF setting means that SPI master will insert delay between each transmitting data, but the /CS remain LOW between two transfer, the Frame Delay time is defined in SPI Delay register.

The EOT setting means that SPI master will insert delay between each transmitting data, meanwhile the /CS is driven to HIGH between two transfer, the Transfer Delay time is defined in SPI Delay register. That the /CS is set high means that the transfer is completed.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信