LPC4370 GPIO DMA Request

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4370 GPIO DMA Request

1,715件の閲覧回数
aliasadzadeh
Contributor II

Hi,

I have read the user manual, but unfortunately there is no DMA request lines from GPIO, I have some signals hooked up to the PIN P1_3 or GPIO0[10], I want to know is there any kinda trick or use of other peripherals to trig the DMA request on that pin? why there is no DMA request on Normal GPIO pins? is there any way?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,483件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the following threads:

Transfer data from parallel GPIO using GPDMA 

How to transfer the data between the GPIO port to internal memory SRAM in LPC4370 without using the ... 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信