LPC4370 GPIO DMA Request

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4370 GPIO DMA Request

1,717 Views
aliasadzadeh
Contributor II

Hi,

I have read the user manual, but unfortunately there is no DMA request lines from GPIO, I have some signals hooked up to the PIN P1_3 or GPIO0[10], I want to know is there any kinda trick or use of other peripherals to trig the DMA request on that pin? why there is no DMA request on Normal GPIO pins? is there any way?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,485 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the following threads:

Transfer data from parallel GPIO using GPDMA 

How to transfer the data between the GPIO port to internal memory SRAM in LPC4370 without using the ... 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply