LPC4337 multiple flash Hardfault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4337 multiple flash Hardfault

1,479件の閲覧回数
mallikarjunared
Contributor III

Hi,

         I am trying to interface external flash with LPC4337 controller.  Please find below information for your reference.

  

         Board : LPCxpresso 4337

         Flash chip : onboard MX25L8035E

         Example code : LPC4337_multiple_flash (download link : https://www.lpcware.com/content/faq/lpcxpresso/configuring-projects-multiple-flash).

        

        I am getting Hardfault, when i use Flash3. It is working fine in case of Flash2.  Can someone help on this.

Thanks & Regards,

Mallikarjun

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 返信

1,335件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mallikarjun,

I think it's Ok to ignore the thread, and I've already given the reply in the LPC4337 SPIFI MX23L8035 not working .
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信