LPC214x USB problem with sleep mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC214x USB problem with sleep mode

1,984件の閲覧回数
guillaumelesieu
Contributor II

I'm working with the MCU LPC214x (LPC2141) with Windows 7, 64 bit.

I use a usb driver on the MCU and the usb driver lpc-ucom-vcom.inf provide by NXP for windows 7.

I have a problem with the sleep mode. When the microcontroller is connected by USB with the computer and the computer goes to sleep,
I have this error (BUGCODE_USB_DRIVER, 0X000000FE (0x04,0xFFFFFA8016F19010,0xFFFFFA801888600,0x0FFFFFA801AD92950)

pastedImage_1.jpg


The proporties of the usb driver on the MCU are :


Power management features:
00000019
PDCAP_D0_SUPPORTED
PDCAP_D3_SUPPORTED
PDCAP_WAKE_FROM_D0_SUPPORTED


I think the problem comes from the usb driver on the MCU.

I would like to know if the problem comes from the driver on the mcu or on windows.

 
Thanks in advance.


Best regards.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,790件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Lesieur,

It may me also related to the version of USB controller divers included by Windows. You could take a look to the following links:

https://answers.microsoft.com/en-us/windows/forum/windows_7-hardware/blue-screen-on-hibernatesuspend...

https://community.nxp.com/thread/309556


Hope this will be useful for you.
Best regards!
/Carlos

0 件の賞賛
返信