The Lpc4330 can’t boot from spifi flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The Lpc4330 can’t boot from spifi flash

1,694 Views
pengdacheng
Contributor I

I am using the OM13027: LPC4330-Xplorer Board,which I can found that it is flashless and  use the external flash S25FL032P0XMFI013. I download some example project from nxp websit and generate the binary files. After I program the external flash and turn off the power, when I repower the board the lpc4330 can not boot from the spifi flash.  I had set the boot mode right but I don't know why it can't still boot from external flash.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,573 Views
miguel_mendoza
NXP Employee
NXP Employee

Hi peng dacheng,

Could you give me more information about what example are you trying to prove, are you using the LPCOpen examples?

regards,
Miguel Mendoza

0 Kudos
Reply