LPC2103 GPIO pin High/Low

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC2103 GPIO pin High/Low

2,119件の閲覧回数
eswarchand
Contributor I

Hi,

   I am new to LPC2103. i bought this LPC2103 Controller for my project purpose.in this first i need to high/low the gpio pin.i saw the user manual provided in NXP.i saw the registers used for  GPIO. i used PINSEL,IODIR,IOCLR,IOSET registers.these registers are enough or any other registers are required for GPIO pin High/Low because i wrote the code using these registers and downloaded the code to micro controller through Python chip programmer.the code is downloaded but it is not working.

please let me know what else are required.

thank you

Eshwar

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,734件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Eshwar,

Have you ensured that the programmer was able to properly download the code? The proper registers for GPIO manipulation are explained on Chapter 8 “LPC2101/02/03 General Purpose Input/Output ports (GPIO)” of the “LPC2101/02/03 User manual”

You could also refer to the following GPIO tutorial for LPC2148:

http://www.ocfreaks.com/lpc2148-gpio-programming-tutorial/

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信