LPC1788FBD208 Pin compatible

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC1788FBD208 Pin compatible

跳至解决方案
2,458 次查看
Childe
Contributor II

Dear All,

I understand NXP just released LPC546xx. I saw specification of this part can be upgraded for LPC1788FBD208. Does LPC546xx have part number which is pin to pin compatible with LPC1788FBD208? 

Regard,

Wittawas

标签 (3)
0 项奖励
回复
1 解答
2,261 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Wittawas,

The LPC546xx does not have a pin to pin compatible part number with the LPC1788FBD208 but the LPC408x is pin compatible with LPC1778x with enhancements in the core and advanced peripherals. The following application note highlights some of the differences between these two families and provides guidance when switching from the LPC178x based hardware/software to the LPC408x systems:

http://cache.nxp.com/documents/application_note/AN11335.zip


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

在原帖中查看解决方案

1 回复
2,262 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Wittawas,

The LPC546xx does not have a pin to pin compatible part number with the LPC1788FBD208 but the LPC408x is pin compatible with LPC1778x with enhancements in the core and advanced peripherals. The following application note highlights some of the differences between these two families and provides guidance when switching from the LPC178x based hardware/software to the LPC408x systems:

http://cache.nxp.com/documents/application_note/AN11335.zip


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer