LPC1788FBD208 Pin compatible

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788FBD208 Pin compatible

Jump to solution
2,404 Views
Childe
Contributor II

Dear All,

I understand NXP just released LPC546xx. I saw specification of this part can be upgraded for LPC1788FBD208. Does LPC546xx have part number which is pin to pin compatible with LPC1788FBD208? 

Regard,

Wittawas

Labels (3)
0 Kudos
Reply
1 Solution
2,207 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Wittawas,

The LPC546xx does not have a pin to pin compatible part number with the LPC1788FBD208 but the LPC408x is pin compatible with LPC1778x with enhancements in the core and advanced peripherals. The following application note highlights some of the differences between these two families and provides guidance when switching from the LPC178x based hardware/software to the LPC408x systems:

http://cache.nxp.com/documents/application_note/AN11335.zip


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

View solution in original post

1 Reply
2,208 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Wittawas,

The LPC546xx does not have a pin to pin compatible part number with the LPC1788FBD208 but the LPC408x is pin compatible with LPC1778x with enhancements in the core and advanced peripherals. The following application note highlights some of the differences between these two families and provides guidance when switching from the LPC178x based hardware/software to the LPC408x systems:

http://cache.nxp.com/documents/application_note/AN11335.zip


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer