LPC1788 Using USB Host Lite to Drive USB to Serial Dongle PL2303

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 Using USB Host Lite to Drive USB to Serial Dongle PL2303

1,000件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dennisyeung on Wed Jun 11 20:04:02 MST 2014
Hi All,

Do anyone have the source code for using LPC1788 USB Host to drive the USB to Serial Dongle like PL2303?

I prefer it to use USB Host Lite to drive PL2303 if possible.

BR
Dennis
ラベル(1)
0 件の賞賛
返信
1 返信

926件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Jun 20 12:47:03 MST 2014
Hi, Dennis,

You might refer to the USB_HostLite sample project from below link:
http://www.lpcware.com/content/nxpfile/lpc177x-and-lpc178x-cmsis-compliant-standard-peripheral-firmw...

regards,
0 件の賞賛
返信