LPC1788 Using USB Host Lite to Drive USB to Serial Dongle PL2303

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 Using USB Host Lite to Drive USB to Serial Dongle PL2303

997 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dennisyeung on Wed Jun 11 20:04:02 MST 2014
Hi All,

Do anyone have the source code for using LPC1788 USB Host to drive the USB to Serial Dongle like PL2303?

I prefer it to use USB Host Lite to drive PL2303 if possible.

BR
Dennis
标签 (1)
0 项奖励
回复
1 回复

923 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Jun 20 12:47:03 MST 2014
Hi, Dennis,

You might refer to the USB_HostLite sample project from below link:
http://www.lpcware.com/content/nxpfile/lpc177x-and-lpc178x-cmsis-compliant-standard-peripheral-firmw...

regards,
0 项奖励
回复