LPC1788 Using USB Host Lite to Drive USB to Serial Dongle PL2303

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 Using USB Host Lite to Drive USB to Serial Dongle PL2303

1,006 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dennisyeung on Wed Jun 11 20:04:02 MST 2014
Hi All,

Do anyone have the source code for using LPC1788 USB Host to drive the USB to Serial Dongle like PL2303?

I prefer it to use USB Host Lite to drive PL2303 if possible.

BR
Dennis
Labels (1)
0 Kudos
Reply
1 Reply

932 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Jun 20 12:47:03 MST 2014
Hi, Dennis,

You might refer to the USB_HostLite sample project from below link:
http://www.lpcware.com/content/nxpfile/lpc177x-and-lpc178x-cmsis-compliant-standard-peripheral-firmw...

regards,
0 Kudos
Reply