LPC1768 replacing LPC2368

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 replacing LPC2368

Jump to solution
2,288 Views
Savelec
Contributor I

Hi,

I want to use the LPC1768 in replacement for the LPC2368 on existing electronic boards. 

The pin n°13 on LPC2368 (LQFP100 package) must be connected to Vdd (3.3V) but the pin in "not connected" on LPC1768.

Can I still leave this pin to Vdd on LPC1768 or this pin must be not connected ?

Thanks

0 Kudos
Reply
1 Solution
2,271 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @Savelec 

the LPC1768 is a replacement for the LPC2368.

Regarding to the pin, LPC1768 pin13 is nc while LPC2368 connects to Vdd. The LPC1768 and the LPC2368 are not strictly pin-compatible. However it's possible to directly replace a LPC2368 with an LPC1768/66 (at the same board.).In this case it's no problem to connect the NC pin 13 of the LPC1768 to Vdd

However, please note the longevity of LPC1766/8/9 are less than 5 years left. We don’t have other pin to pin replacement longer than10 years.

 

Hope this helps.

Jun Zhang

View solution in original post

0 Kudos
Reply
2 Replies
2,267 Views
Savelec
Contributor I

Hi Jun Zhang

Many thanks, this is the answer i was waiting for !

Have a nice day.

0 Kudos
Reply
2,272 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @Savelec 

the LPC1768 is a replacement for the LPC2368.

Regarding to the pin, LPC1768 pin13 is nc while LPC2368 connects to Vdd. The LPC1768 and the LPC2368 are not strictly pin-compatible. However it's possible to directly replace a LPC2368 with an LPC1768/66 (at the same board.).In this case it's no problem to connect the NC pin 13 of the LPC1768 to Vdd

However, please note the longevity of LPC1766/8/9 are less than 5 years left. We don’t have other pin to pin replacement longer than10 years.

 

Hope this helps.

Jun Zhang

0 Kudos
Reply