LPC1768 - UART using DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 - UART using DMA

Jump to solution
5,992 Views
tomasfrcek
Contributor III

Hello,

is there an example code demonstrating the UART receive and transmit using the DMA?

Thanks!

Tomas F.

Labels (1)
0 Kudos
Reply
1 Solution
5,004 Views
soledad
NXP Employee
NXP Employee

Hi, 

Please check the following links: 

CMSIS Example Code: UART/DMA/uart_dma_test.c Source File 

LPC1778, Problems with UART Rx DMA Transfer 

Enable DMA in LPC1768 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
5,005 Views
soledad
NXP Employee
NXP Employee

Hi, 

Please check the following links: 

CMSIS Example Code: UART/DMA/uart_dma_test.c Source File 

LPC1778, Problems with UART Rx DMA Transfer 

Enable DMA in LPC1768 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
5,004 Views
tomasfrcek
Contributor III

Thank you, very useful links!

0 Kudos
Reply