LPC1768 - UART using DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC1768 - UART using DMA

跳至解决方案
6,106 次查看
tomasfrcek
Contributor III

Hello,

is there an example code demonstrating the UART receive and transmit using the DMA?

Thanks!

Tomas F.

标签 (1)
0 项奖励
回复
1 解答
5,118 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Please check the following links: 

CMSIS Example Code: UART/DMA/uart_dma_test.c Source File 

LPC1778, Problems with UART Rx DMA Transfer 

Enable DMA in LPC1768 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
5,118 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Please check the following links: 

CMSIS Example Code: UART/DMA/uart_dma_test.c Source File 

LPC1778, Problems with UART Rx DMA Transfer 

Enable DMA in LPC1768 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
5,118 次查看
tomasfrcek
Contributor III

Thank you, very useful links!

0 项奖励
回复