LPC1317 GPIO Interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1317 GPIO Interrupts

1,523件の閲覧回数
lorenzogalbiati
Contributor I

Hello,

I'm developing a new product with this microcontroller and I want to use GPIO external interrupt. I can't find how to reset the interrupt flag in order to clear the interrupt request inside the interrupt service routine. For other interrupts I have found that it's possible to write one's in flag in order to clear the flag but with these GPIO interrupt I can't find anything and the datasheet doesn't report anything or I'm not able to fint this info.

Can anyone help me?

Many thanks.

0 件の賞賛
返信
1 返信

1,518件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport
 

 



Dear Lorenzo Galbiati,

I do not know if you use PIN interrupt or group interrupt.
If you use pin interrupt, you can check the section 9.5.1.10 Pin interrupt status register (IST address 0x4004 C024) , there are 8 pin interrupt source, each pin interrupt corresponds to one bit in the register. Writing 1 to the corresponding bit clears the bit in IST and corresponding the rising or falling edge registers.

For example PINTSEL0 corresponds to bit0 of IST, PINTSEL1 corresponds to bit1 of IST...

If you use GROUPx interrupt, pls refer to section 9.5.2.1 Grouped interrupt control register.
The INT bit of "GPIO grouped interrupt control register" reflects the interrupt status bit, you can write 1 to clear the bit.
Hope it can help you.

BR

XiangJun Rong

0 件の賞賛
返信