LPC11E68 Serial port 3 RX interrupt.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11E68 Serial port 3 RX interrupt.

ソリューションへジャンプ
8,668件の閲覧回数
sirurx
Contributor III

Hi,

I'm using LPC11E68 Serial port 3. I am failing to get interrupt on RX. I can see that LPC_USART3.RXDATA fills with data but INTSTAT stays 0, and  USART2_3_IRQn is never called.

What i'm starting with is:

Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_IOCON);

Chip_GPIO_Init(LPC_GPIO);

Chip_Clock_SetUSARTNBaseClockRate((115200 * 48), true);

Chip_IOCON_PinMuxSet(LPC_IOCON, 2, 3, (IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGMODE_EN));

Chip_IOCON_PinMuxSet(LPC_IOCON, 2, 4, (IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGMODE_EN));

Chip_UARTN_Init(LPC_USART3);

Chip_UARTN_ConfigData(LPC_USART3, UARTN_CFG_DATALEN_8 | UARTN_CFG_PARITY_NONE | UARTN_CFG_STOPLEN_1);

Chip_UARTN_SetBaud(LPC_USART3, 115200);

Chip_UARTN_Enable(LPC_USART3);

Chip_UARTN_TXEnable(LPC_USART3);

Chip_UARTN_IntEnable(LPC_USART3, UARTN_INTEN_RXRDY);

Chip_UARTN_IntDisable(LPC_USART3, UARTN_INTEN_TXRDY);

NVIC_EnableIRQ(USART2_3_IRQn);

After that i'm having in LPC_USART3:

CFG=b101 (5) - does not change any time later. USART ENABE=1; 8N1; async.

CTRL=0 - does not change. normal operation, no autobaud.

STAT= b11110 on startup: RX is idle and no incoming, can send, tx idle,CTS=1.

INTENSET=1: RXRDYEN=1 - shall generate interrupt when RXDAT has data.

INTENCLR=0: - used for clearuig INTENSET bits, so hall be 0.

BRG=(2): The FRG clock is divided by 3 before use by the USART function.

INTSTAT=0: - this shall show when interrupt occurs?

OSR=b1111 (15): 16 peripheral clocks are used to transmit and receive each data bit.

ADDR=0, this is not used, as ADDRDET=0;

Checked that SYSAHBCLKCTRL bit 22 is set.

Then i'm sending data to modem and can see RXDATA and RXDATASTAT changes after modem answers.

Data seems to be correct there.

So this is seemingly not i/o level or pin configuration issue.

What i'm missing?

BR,

Ergo

ラベル(2)
0 件の賞賛
返信
1 解決策
8,228件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ergo,

Oh gosh, the code seems to be complicated.

I've attached a simple demo which about the sending and receiving message with USART0/1, and please refer to it for details.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
12 返答(返信)
8,229件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ergo,

Oh gosh, the code seems to be complicated.

I've attached a simple demo which about the sending and receiving message with USART0/1, and please refer to it for details.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
8,228件の閲覧回数
sirurx
Contributor III

Hi Ping,

I checked out your code and basically it was same as mine so i started to wonder what else could be wrong.

I commented out USART0 functions and interrupt works now.

I would say that the current topic is closed but i will investigate how the using of two serials in same time affect interrupts.

It might be interrupt priority issue.

Anyway thank you for your support and i will follow the rabbit hole :smileyhappy:

BR,

Ergo

0 件の賞賛
返信
8,228件の閲覧回数
sirurx
Contributor III

Hi Ping,

Thanx. I will check out your example.

If still having an issue, i will trim down my code to point that it's minimalistic :smileyhappy:

BR,

Ergo

0 件の賞賛
返信
8,228件の閲覧回数
sirurx
Contributor III

New findings: When i use external serial data then first character never gets interrupt, only starting from second character.
For loopback situation it never gets interrupt.

0 件の賞賛
返信
8,228件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ergo,

Thanks for your reply.

I was wondering if you can share the whole the demo and what evaluation you run on, then I can replicate the issue on my site and accelerate to figure out the root cause.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
8,228件の閲覧回数
sirurx
Contributor III

Hi Ping,

I am using custom PCB. MCU is LPC11E68JBD48 There is two USART-s in use.

USART0 is connected to outside world through USB to SERIAL converter. Currently connected to PC, running terminal program (Putty).

USART1 (or USART3) is connected to modem(through level converters). Currently i disconnected it from modem and connected RX and TX together to form loopback. Also i can measure signal from there with scope.

MCU is running at 48MHz, Redlib(none), No optimizations. Pasted code below.

//----------------------------------------------------------------------------------------------------------------------

//main.c:

#include "chip.h"

#include <stdio.h>

#include <define.h>

#include "debug.h"

#include "modem.h"

#include "time.h"

volatile static int32_t ticks;

volatile static uint8_t rtcWake, rtcAlarm;

volatile static uint8_t us_timeout;

void SysTick_Handler(void)

{

    ticks++;

}

void system_pause(uint32_t pause_ms)

{

    int32_t last_ticks;

    while (pause_ms)

    {

        last_ticks = ticks;

        while(last_ticks == ticks);

        pause_ms--;

    }

}

void InitSysTick()

{

    // Enable SysTick Timer, block if failed, this shall trigger WDT reset in future

       if(SysTick_Config(SystemCoreClock / TICKRATE_HZ))

       {

           while(1);

       }

}

int main(void)

{

    uint32_t i;

    //uint8_t buf[RESPONSE_BUFF_ITEM_SIZE+10];

    //uint8_t b2[5], j;

    void * pbuf;

    // Read clock settings and update SystemCoreClock variable

    SystemCoreClockUpdate();

    //Enable IOCON clock - needed for Pinmux command

    Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_IOCON);

    Chip_GPIO_Init(LPC_GPIO);

    //Init systick timer for delays

    InitSysTick();

    InitDebugSerial();

    PrintLog("\r\nTesting modem uart\r\n");

    ModemInit();

    while (1) {

        pbuf = debug_read_response();

        if (pbuf != NULL)

        {

            ModemSendCommand(pbuf);

            debug_responses_clear();

            ModemSendCommand("\r\n");

            //ModemSendCommand("a");

        }

        system_pause(1);

        for (i = 0; i < RESPONSE_BUFF_SIZE; i++) {

            pbuf = read_response((uint8_t) i);

            if (pbuf != NULL) {

                PrintLog(pbuf);

                PrintLog("\r\n");

                mark_response_read(i);

            }

        }

    }

}

//----------------------------------------------------------------------------------------------------------------------

/*

* debug.c

*

*  Created on: 16. juuni 2016

*      Author: ergo

*/

#include "debug.h"

#include "time.h"

volatile static char debug_rx_buffer[DEBUG_RX_BUFF_SIZE];

volatile static int16_t debug_rx_buffer_len = 0;

volatile static uint8_t debug_handling_rx = 0;

volatile static RESPONSE_LINE_T debug_response_buffer[DEBUG_RESPONSE_BUFF_SIZE]; //52*39 = 2028bytes

void debug_responses_clear()

{

    uint32_t i;

    NVIC_DisableIRQ(MODEM_USART_IRQNUM);

    //wait until rx receive procedure ends

    while(debug_handling_rx)

        system_pause(1);

    debug_rx_buffer_len = 0;

    for(i=0; i< DEBUG_RESPONSE_BUFF_SIZE; i++)

    {

        debug_response_buffer[i].r_new = 0;

    }

    NVIC_EnableIRQ(DEBUG_USART_IRQNUM);

}

void debug_response_add(char *s)

{

    uint32_t i, len;

    uint8_t result;

    result = 0;

    len = strlen(s);

    //If string is too long, truncate

    if(len > (RESPONSE_BUFF_ITEM_SIZE -1))

            len = RESPONSE_BUFF_ITEM_SIZE -1;

    //Copy response to first free slot as we don't care about response order

    for(i=0; i< DEBUG_RX_BUFF_SIZE; i++)

    {

        if(debug_response_buffer[i].r_new == 0)

        {

            memcpy((char*)&debug_response_buffer[i].data,s,len);

            debug_response_buffer[i].data[len] = '\0';

            debug_response_buffer[i].r_new = 1;

            result = 1;

            break;

        }

        //If buffer is full, new item is ignored at moment

    }

    if(result == 0)

    {

        PrintLog("ERROR: debug_response_buffer full\r\n");

    }

}

char * debug_read_response()

{

    if(debug_response_buffer[0].r_new != 1)

            return NULL;

    return debug_response_buffer[0].data;

}

void debug_update_rx_buffer(uint8_t db) {

    if ((db == (char) 0x0D) || (db == (char) 0x0A) || (db == (char) 0)) {

        if (debug_rx_buffer_len > 0) {

            debug_rx_buffer[debug_rx_buffer_len] = (char) 0;

            debug_response_add(debug_rx_buffer);

            debug_rx_buffer_len = 0;

        }

    } else if (debug_rx_buffer_len <= (MODEM_RX_BUFF_SIZE - 1)) {

        debug_rx_buffer[debug_rx_buffer_len] = (char) db;

        debug_rx_buffer_len++;

    }

}

void USART0_IRQHandler(void)

{

    uint32_t IIRValue, LSRValue;

    uint8_t Dummy;

    debug_handling_rx = 1;

    IIRValue = DEBUG_UART->IIR;

    if(IIRValue & UART0_IIR_INTID_RLS)

    {

        LSRValue = DEBUG_UART->LSR;

        if (LSRValue & (LSR_OE | LSR_PE | LSR_FE | LSR_RXFE | LSR_BI))

        {

            Dummy = (uint8_t)DEBUG_UART->RBR;    // Dummy read on RX to clear interrupt

            debug_handling_rx = 0;

            return;

        }

        if (LSRValue & LSR_RDR)    // Receive Data Ready

        {

            debug_update_rx_buffer((uint8_t)DEBUG_UART->RBR);

        }

    }

    else if(IIRValue & UART0_IIR_INTID_RDA)

    {

        debug_update_rx_buffer((uint8_t)DEBUG_UART->RBR);

    }

    else if(IIRValue & UART0_IIR_INTID_CTI)

    {

        //Character timeout indicator

    }

    else if(IIRValue & UART0_IIR_INTID_THRE)

    {

        //THRE, transmit holding register empty

    }

    //LPC_UART0D_API->uart_isr(uartHandle);

    debug_handling_rx = 0;

}

void InitDebugSerial()

{

    debug_responses_clear();

    debug_rx_buffer_len = 0;

    debug_handling_rx = 0;

    //Chip_Clock_SetUSARTNBaseClockRate((DEBUG_UART_SPEED * 48), true);

    Chip_IOCON_PinMuxSet(LPC_IOCON, IO_ISP_RX.Port, IO_ISP_RX.Pin, IO_ISP_RX.Mode);

    Chip_IOCON_PinMuxSet(LPC_IOCON, IO_ISP_TX.Port, IO_ISP_TX.Pin, IO_ISP_TX.Mode);

    Chip_UART0_Init(DEBUG_UART);

    Chip_UART0_SetBaud(DEBUG_UART, DEBUG_UART_SPEED);

    Chip_UART0_ConfigData(DEBUG_UART, (UART0_LCR_WLEN8 | UART0_LCR_SBS_1BIT));

    //Chip_UART0_SetupFIFOS(DEBUG_UART, (UART0_FCR_FIFO_EN | UART0_FCR_TRG_LEV2));

    Chip_UART0_TXEnable(DEBUG_UART);

    Chip_UART0_IntEnable(DEBUG_UART, UARTN_INTEN_RXRDY);

    NVIC_EnableIRQ(DEBUG_USART_IRQNUM);

}

void PrintLog(char *str)

{

    uint32_t len;

    len = strlen(str);

    while (len != 0)

    {

        while ( !(DEBUG_UART->LSR & LSR_THRE) );

        DEBUG_UART->THR = *str;

        str++;

        len--;

        //Chip_UART0_SendByte(DEBUG_UART, *str++);

    }

}

//----------------------------------------------------------------------------------------------------------------------

//modem.c

/*

* Modem functions

* */

#include "define.h"

#include "time.h"

#include "debug.h"

volatile static char modem_rx_buffer[MODEM_RX_BUFF_SIZE];

volatile static int16_t modem_rx_buffer_len = 0;

volatile static uint8_t modem_handling_rx = 0;

volatile static RESPONSE_LINE_T response_buffer[RESPONSE_BUFF_SIZE]; //52*39 = 2028bytes

const char* LF = "\r\n";

void responses_clear()

{

    uint32_t i;

    while(modem_handling_rx)

        system_pause(1);

    modem_rx_buffer_len = 0;

    for(i=0; i< RESPONSE_BUFF_SIZE; i++)

    {

        response_buffer[i].r_new = 0;

    }

}

void response_add(char *s)

{

    uint32_t i, len;

    uint8_t result;

    result = 0;

    len = strlen(s);

    //If string is too long, truncate

    if(len > (RESPONSE_BUFF_ITEM_SIZE -1))

            len = RESPONSE_BUFF_ITEM_SIZE -1;

    //Copy response to first free slot as we don't care about response order

    for(i=0; i< RESPONSE_BUFF_SIZE; i++)

    {

        if(response_buffer[i].r_new == 0)

        {

            memcpy((char*)&response_buffer[i].data,s,len);

            response_buffer[i].data[len] = '\0';

            response_buffer[i].r_new = 1;

            result = 1;

            break;

        }

        //If buffer is full, new item is ignored at moment

    }

    if(result == 0)

    {

        PrintLog("ERROR: response_buffer full\r\n");

    }

}

//Searches first response containing strin filter

//marks it as read/cleared if mark_as_read set

//returns index of matching response, if not found, return 0xff

uint8_t find_response(char * filter, bool mark_as_read)

{

    uint32_t i, flen;

    uint8_t result, idx;

    result = 0;

    flen = strlen(filter);

    for(i=0; i< RESPONSE_BUFF_SIZE; i++)

    {

        if(response_buffer[i].r_new == 1 && flen <= strlen(response_buffer[i].data) && strstr(response_buffer[i].data, filter) != NULL)

        {

            if(mark_as_read)

                response_buffer[i].r_new = 0;

            idx = i;

            result = 1;

            break;

        }

    }

    if(result)

        return idx;

    else

        return 0xff;

}

//Searches response containing strin filter

//marks these as read/cleared if mark_as_read set

//returns count of matching responses

uint8_t find_responses(char * filter, bool mark_as_read)

{

    uint32_t i, flen;

    uint8_t count;

    count = 0;

    flen = strlen(filter);

    for(i=0; i< RESPONSE_BUFF_SIZE; i++)

    {

        if(response_buffer[i].r_new == 1 && flen <= strlen(response_buffer[i].data) && strstr(response_buffer[i].data, filter) != NULL)

        {

            if(mark_as_read)

                response_buffer[i].r_new = 0;

            count++;

        }

    }

    return count;

}

//Return response data pointer by id

char * read_response(uint8_t id)

{

    if(response_buffer[id].r_new != 1)

        return NULL;

    return response_buffer[id].data;

}

void mark_response_read(uint8_t id)

{

    response_buffer[id].r_new = 0;

}

//Adds symbols to RX buffer rxCommandBuff until new line symbol or 0 received.

//If new line, then adds content of RX buffer to response list with Response_Add() function and resets RX buf len

void update_rx_buffer(uint8_t db) {

    if ((db == (char) 0x0D) || (db == (char) 0x0A) || (db == (char) 0)) {

        if (modem_rx_buffer_len > 0) {

            modem_rx_buffer[modem_rx_buffer_len] = (char) 0;

            response_add(modem_rx_buffer);

            modem_rx_buffer_len = 0;

        }

    } else if (modem_rx_buffer_len <= (MODEM_RX_BUFF_SIZE - 1)) {

        modem_rx_buffer[modem_rx_buffer_len] = (char) db;

        modem_rx_buffer_len++;

    }

}

//void USART2_3_IRQHandler(void)

void USART1_4_IRQHandler(void)

{

    uint32_t IIRValue, LSRValue;

    //uint8_t Dummy;

    modem_handling_rx = 1;

    IIRValue = MODEM_USART->INTSTAT;

    if(IIRValue == UARTN_INTEN_RXRDY)

    {

        update_rx_buffer((uint8_t) MODEM_USART->RXDATA & 0x000001FF);

    }

    /*

    if (IIRValue & UART0_IIR_INTID_RLS) {

        LSRValue = MODEM_USART->LSR;

        if (LSRValue & (LSR_OE | LSR_PE | LSR_FE | LSR_RXFE | LSR_BI)) {

            Dummy = (uint8_t) MODEM_USART->RBR;// Dummy read on RX to clear interrupt

            return;

        }

        if (LSRValue & LSR_RDR)    // Receive Data Ready

        {

            update_rx_buffer((uint8_t) MODEM_USART->RBR);

        }

    } else if (IIRValue & UART0_IIR_INTID_RDA) {

        update_rx_buffer((uint8_t) MODEM_USART->RBR);

    } else if (IIRValue & UART0_IIR_INTID_CTI) {

        //Character timeout indicator

    } else if (IIRValue & UART0_IIR_INTID_THRE) {

        //THRE, transmit holding register empty

    }

    //Chip_UARTN_IRQRBHandler(LPC_USART, &rxring, &txring);

    //modem_rx_buffer, modem_rx_buffer_len

    //update_rx_buffer();

*/

    modem_handling_rx = 0;

}

void ModemInit()

{

    responses_clear();

    modem_rx_buffer_len = 0;

    modem_handling_rx = 0;

    NVIC_DisableIRQ(USART1_4_IRQn);

    Chip_Clock_SetUSARTNBaseClockRate((MODEM_USART_BAUD * 48), true);

    Chip_IOCON_PinMuxSet(LPC_IOCON, IO_MDM_RX.Port, IO_MDM_RX.Pin, IO_MDM_RX.Mode);

    Chip_IOCON_PinMuxSet(LPC_IOCON, IO_MDM_TX.Port, IO_MDM_TX.Pin, IO_MDM_TX.Mode);

    Chip_IOCON_PinMuxSet(LPC_IOCON, IO_MDM_RX_RESERV.Port, IO_MDM_RX_RESERV.Pin, IO_MDM_RX_RESERV.Mode);

    Chip_IOCON_PinMuxSet(LPC_IOCON, IO_MDM_TX_RESERV.Port, IO_MDM_TX_RESERV.Pin, IO_MDM_TX_RESERV.Mode);

    Chip_UARTN_Init(MODEM_USART);

    Chip_UARTN_ConfigData(MODEM_USART, UARTN_CFG_DATALEN_8 | UARTN_CFG_PARITY_NONE | UARTN_CFG_STOPLEN_1);

    Chip_UARTN_SetBaud(MODEM_USART, MODEM_USART_BAUD);

    Chip_UARTN_Enable(MODEM_USART);

    Chip_UARTN_TXEnable(MODEM_USART);

    NVIC_EnableIRQ(MODEM_USART_IRQNUM);

    Chip_UARTN_IntEnable(MODEM_USART, UARTN_INTEN_RXRDY);

}

void ModemDeinit()

{

    Chip_UARTN_IntDisable(MODEM_USART, UARTN_INTEN_RXRDY);

    NVIC_DisableIRQ(MODEM_USART_IRQNUM);

    Chip_UARTN_DeInit(MODEM_USART);

    Chip_IOCON_PinMuxSet(LPC_IOCON, IO_MDM_RX.Port, IO_MDM_RX.Pin, IOCON_FUNC0);

    Chip_IOCON_PinMuxSet(LPC_IOCON, IO_MDM_TX.Port, IO_MDM_TX.Pin, IOCON_FUNC0);

}

void ModemSendCommand(uint8_t * s)

{

    uint32_t len;

    uint8_t ch;

    len = strlen(s);

    Chip_UARTN_IntDisable(MODEM_USART, UARTN_INTEN_TXRDY);

    while ( len != 0 )

    {

        while ( !(MODEM_USART->STAT & UARTN_STAT_TXRDY) );

        ch = *s;

        MODEM_USART->TXDATA = ch;

        s++;

        len--;

    }

    Chip_UARTN_IntEnable(MODEM_USART, UARTN_INTEN_TXRDY);

}

//----------------------------------------------------------------------------------------------------------------------

/*

* define.h

*

*  Created on: 17. juuni 2016

*      Author: ergo

*/

#include "chip.h"

#include <stdio.h>

#include <string.h>

#ifndef DEFINE_H_

#define DEFINE_H_

//Replaces define.h

#define BOOLEAN       uint8_t

#define OFF           0

#define ON            1

//Systick timer parameters --------------------------

#define TICKRATE_HZ (1000)    // tick per millisecond

//Debug Serial used to program the device and also put out log for inspection and bug-finding

#define DEBUG_UART LPC_USART0

#define DEBUG_USART_IRQNUM USART0_IRQn

#define DEBUG_UART_SPEED 115200

#define DEBUG_RX_BUFF_SIZE 100

#define DEBUG_RESPONSE_BUFF_SIZE 2

//I/O definitions ---------------------------------------------------------------------

typedef struct io_pin{

    uint8_t Port;

    uint8_t Pin;

    uint32_t Mode;

}IO_PIN_T;

static const struct io_pin IO_ISP_RX = {.Port=0, .Pin=18, .Mode=(IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)};

static const struct io_pin IO_ISP_TX = {.Port=0, .Pin=19, .Mode=(IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)};

//static const struct io_pin IO_MDM_RX = {.Port=2, .Pin=3, .Mode=(IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)};

//static const struct io_pin IO_MDM_TX = {.Port=2, .Pin=4, .Mode=(IOCON_FUNC1 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)};

static const struct io_pin IO_MDM_RX_RESERV = {.Port=2, .Pin=3, .Mode=(IOCON_FUNC0 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)};

static const struct io_pin IO_MDM_TX_RESERV = {.Port=2, .Pin=4, .Mode=(IOCON_FUNC0 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)};

static const struct io_pin IO_MDM_RX = {.Port=0, .Pin=13, .Mode=(IOCON_FUNC4 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)};

static const struct io_pin IO_MDM_TX = {.Port=0, .Pin=14, .Mode=(IOCON_FUNC4 | IOCON_MODE_INACT | IOCON_DIGMODE_EN)};

//#define MODEM_USART LPC_USART3

//#define MODEM_USART_IRQNUM USART2_3_IRQn

//#define MODEM_USART_BAUD 115200

#define MODEM_USART LPC_USART1

#define MODEM_USART_IRQNUM USART1_4_IRQn

#define MODEM_USART_BAUD 115200

#define MODEM_RX_BUFF_SIZE 200

#define RESPONSE_BUFF_ITEM_SIZE 50

//Defines one response line

typedef struct response_line{

    uint8_t r_id;

    uint8_t r_new;

    uint8_t data[RESPONSE_BUFF_ITEM_SIZE];

}RESPONSE_LINE_T;

//Maximum size of received modem response, parsed into lines, separated by 0-s

#define RESPONSE_BUFF_SIZE 39

#define IER_RBR        0x01

#define IER_THRE    0x02

#define IER_RLS        0x04

#define IIR_PEND    0x01

#define IIR_RLS        0x03

#define IIR_RDA        0x02

#define IIR_CTI        0x06

#define IIR_THRE    0x01

#define LSR_RDR        0x01

#define LSR_OE        0x02

#define LSR_PE        0x04

#define LSR_FE        0x08

#define LSR_BI        0x10

#define LSR_THRE    0x20

#define LSR_TEMT    0x40

#define LSR_RXFE    0x80

#endif /* DEFINE_H_ */

//----------------------------------------------------------------------------------------------------------------------

/*

* debug.h

*

*  Created on: 16. juuni 2016

*      Author: ergo

*/

#ifndef DEBUG_H_

#define DEBUG_H_

#include <define.h>

void debug_responses_clear();

char * debug_read_response();

void InitDebugSerial();

void PrintLog(char *);

#endif /* DEBUG_H_ */

//----------------------------------------------------------------------------------------------------------------------

/*

* modem.h

*

*  Created on: 16. juuni 2016

*      Author: ergo

*/

#ifndef MODEM_H_

#define MODEM_H_

void ModemEnablePower(void);

void ModemInit(void);

void ModemDeinit(void);

void ModemSendCommand(uint8_t *);

void responses_clear(void);

void response_add(char *);

uint8_t find_response(char *, bool);

uint8_t find_responses(char *, bool);

char * read_response(uint8_t);

void mark_response_read(uint8_t);

#endif /* MODEM_H_ */

//----------------------------------------------------------------------------------------------------------------------

I cleaned code up a lot but i think there is still lot's of not needed functionality for this test :smileyhappy:

So please ignore as much you need.

BR,

Ergo

0 件の賞賛
返信
8,228件の閲覧回数
sirurx
Contributor III

UPDATE

Same results with USART1.

Also fixed logic level potential issue. So now the level is >=0.9VCC and no change.

0 件の賞賛
返信
8,228件の閲覧回数
sirurx
Contributor III

UPDATE

I found that MCU sends at 9600 baud rate byte with length of 932us and external device 936us. The difference is 0.4%.

Looped back MCU to itself (connected RX and TX pins) - no interrupt!

So what it means that MCU can't recognize it's own data. Tested with 9600 and 115200 baud rates. And yes i checked with scope, the data is actually looped back.

I am getting amazed :smileyshocked:.

0 件の賞賛
返信
8,228件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ergo,

What's the issue going on? And I was wondering if you can describe the current issue in details.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
8,228件の閲覧回数
sirurx
Contributor III

Hi Ping,My latest theory is that by receiving more than 1 byte in series causes the problem - no interrupt. It is maybe because serials 1-4 do not seem to have hardware FIFO. At least it's not mentioned in datasheet.

I'll try to test my theory out soon. Maybe these serials must be used with DMA only?BR,

Ergo

0 件の賞賛
返信
8,228件の閲覧回数
sirurx
Contributor III

UPDATE.

Seems like receiving byte and getting interrupt are separate HW channels on chip.

This means that on i/o pin byte can be received but interrupt still not triggered.

First i thought that RXDATA register change triggers interrupt but it is in more lower level. So NVIC monitors also physical signal not USART registers.

I replaced modem with other serial device and now i'm getting interrupts too. I am investigating further what is the difference between modem and other serial device.

0 件の賞賛
返信
8,228件の閲覧回数
sirurx
Contributor III

I also want to add, that NVIC.ISER = 1000000001000000000000 - ISE_USART2_3, ISE_USART0 are set.

I am using also USART0 and it's RX interrupt works fine. USART0 is used for keyboard interaction only.

0 件の賞賛
返信