LPC116x PIO0_0/Reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC116x PIO0_0/Reset

Jump to solution
2,170 Views
vicens
Contributor I

Hello,

I read on the LPC116x User Manual that the PIO0_0 is configurated as reset by default. Are there any way to change this configuration using the programmer? In Microchip microcontrollers exist that utility wfor the Vpp/nMCLR pin.

Thanks,
Vicens

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,061 Views
soledad
NXP Employee
NXP Employee

Hi,

There is no possible to change this configuration.

Have a great day,

Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,062 Views
soledad
NXP Employee
NXP Employee

Hi,

There is no possible to change this configuration.

Have a great day,

Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,061 Views
vicens
Contributor I

Thanks! 

Vicenç

0 Kudos
Reply