LPC116x PIO0_0/Reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,169件の閲覧回数
vicens
Contributor I

Hello,

I read on the LPC116x User Manual that the PIO0_0 is configurated as reset by default. Are there any way to change this configuration using the programmer? In Microchip microcontrollers exist that utility wfor the Vpp/nMCLR pin.

Thanks,
Vicens

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,060件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

There is no possible to change this configuration.

Have a great day,

Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,061件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

There is no possible to change this configuration.

Have a great day,

Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,060件の閲覧回数
vicens
Contributor I

Thanks! 

Vicenç

0 件の賞賛
返信