LPC Pinmux Utility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC Pinmux Utility

跳至解决方案
4,616 次查看
rogerlittlewood
Contributor I

Using the LPC Pinmux utility. It exits with Java error 13. Why?

标记 (1)
0 项奖励
回复
1 解答
4,172 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

If your machine has Java 32 bit installed (which many 64 bit systems seem to), just download  and use the 32 bit version of the LPC Initialization tool. The only real difference is the VM they expect your system to have available.

Regards,

LPCXpresso Support

在原帖中查看解决方案

0 项奖励
回复
6 回复数
4,173 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

If your machine has Java 32 bit installed (which many 64 bit systems seem to), just download  and use the 32 bit version of the LPC Initialization tool. The only real difference is the VM they expect your system to have available.

Regards,

LPCXpresso Support

0 项奖励
回复
4,172 次查看
rogerlittlewood
Contributor I

That worked, thanks for your help.

I couldn't help noticing how complex this simple thing is in terms of software, in my install of this 144 files in 64 folders!! Why couldn't it just be a simple .exe executable?

Regards   ---   Roger

0 项奖励
回复
4,172 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

I assume that you have downloaded the Win64 bit version of the standalone version of the LPC Initialization Tool|NXP ?

The error message you are seeing would normally indicate that the Java virtual machine being found on your machine is actually the 32 bit version rather than the 64 bit version.

If you wish to use the standalone version of this tool (rather than the online version), then you will need to either download the Win32 version of the tool to match your 32-bit Java VM, or else install the 64 bit version of the Java VM. If you do the later, then you may find that you need to modify the lpcinit.ini file within the tool directory to point to the right VM version.

For more background, use your favourite search engine to look for exact text of the java error 13 message that you see.

Regards,

LPCXpresso Support

0 项奖励
回复
4,172 次查看
rogerlittlewood
Contributor I

Yes I installed the 64 bit version of the tool. When I installed Java, there appeared to be no option to select 32/64 bit.

Here is my lpciniti.ini file:

-startup
plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar
--launcher.library
plugins/org.eclipse.equinox.launcher.win32.win32.x86_64_1.1.200.v20150204-1316
-vmargs
-d32

what do I change??

Regards   ---   Roger

0 项奖励
回复
4,172 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Can you let us know what platform you are running on, and what Java version?

0 项奖励
回复
4,172 次查看
rogerlittlewood
Contributor I

Hi Brendon, Sorry for the delay. I'm using Win 10 64 bit and Java Version 8 Update 101 Build 1.0.0_101-b13

0 项奖励
回复