LPC Pinmux Utility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,830件の閲覧回数
rogerlittlewood
Contributor I

Using the LPC Pinmux utility. It exits with Java error 13. Why?

タグ(1)
0 件の賞賛
返信
1 解決策
4,386件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

If your machine has Java 32 bit installed (which many 64 bit systems seem to), just download  and use the 32 bit version of the LPC Initialization tool. The only real difference is the VM they expect your system to have available.

Regards,

LPCXpresso Support

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,386件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

If your machine has Java 32 bit installed (which many 64 bit systems seem to), just download  and use the 32 bit version of the LPC Initialization tool. The only real difference is the VM they expect your system to have available.

Regards,

LPCXpresso Support

0 件の賞賛
返信
4,386件の閲覧回数
rogerlittlewood
Contributor I

That worked, thanks for your help.

I couldn't help noticing how complex this simple thing is in terms of software, in my install of this 144 files in 64 folders!! Why couldn't it just be a simple .exe executable?

Regards   ---   Roger

0 件の賞賛
返信
4,386件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

I assume that you have downloaded the Win64 bit version of the standalone version of the LPC Initialization Tool|NXP ?

The error message you are seeing would normally indicate that the Java virtual machine being found on your machine is actually the 32 bit version rather than the 64 bit version.

If you wish to use the standalone version of this tool (rather than the online version), then you will need to either download the Win32 version of the tool to match your 32-bit Java VM, or else install the 64 bit version of the Java VM. If you do the later, then you may find that you need to modify the lpcinit.ini file within the tool directory to point to the right VM version.

For more background, use your favourite search engine to look for exact text of the java error 13 message that you see.

Regards,

LPCXpresso Support

0 件の賞賛
返信
4,386件の閲覧回数
rogerlittlewood
Contributor I

Yes I installed the 64 bit version of the tool. When I installed Java, there appeared to be no option to select 32/64 bit.

Here is my lpciniti.ini file:

-startup
plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar
--launcher.library
plugins/org.eclipse.equinox.launcher.win32.win32.x86_64_1.1.200.v20150204-1316
-vmargs
-d32

what do I change??

Regards   ---   Roger

0 件の賞賛
返信
4,386件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Can you let us know what platform you are running on, and what Java version?

0 件の賞賛
返信
4,386件の閲覧回数
rogerlittlewood
Contributor I

Hi Brendon, Sorry for the delay. I'm using Win 10 64 bit and Java Version 8 Update 101 Build 1.0.0_101-b13

0 件の賞賛
返信