LPC 54018 Debug Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 54018 Debug Issue

Jump to solution
2,693 Views
yashbohra80
Contributor I

I am trying to program LPC 54018 IOT Module using MCU IDE using PE Micro but when I try to debug a sample LED Blinky program,I get an error message saying that error in FLASH PROGRAM . terminate debug session.

In getting started session i checked i need to update qc firmware file , but while trying to do so I am not able to find qc firmware update file in SDK Version 2.5

Tags (1)
0 Kudos
Reply
1 Solution
2,600 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi yash bohra 

Not sure if I correctly understand your questions. Do you mean your IDE debugger can't launch debugger?

If so, you can try update on board debug firmware with referring this thread.

LPC54608 board doesnt see any debug probes  


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,601 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi yash bohra 

Not sure if I correctly understand your questions. Do you mean your IDE debugger can't launch debugger?

If so, you can try update on board debug firmware with referring this thread.

LPC54608 board doesnt see any debug probes  


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,600 Views
yashbohra80
Contributor I

Hi ,

Thank you for your response. It is working now, there was some problem with USB.

0 Kudos
Reply
2,600 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome.

0 Kudos
Reply