Incorrect LCDFP and LCDLP states with LCDEN disabled.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Incorrect LCDFP and LCDLP states with LCDEN disabled.

763 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GregDavies on Wed Sep 16 08:35:44 MST 2015
In the user manual for the LCD Control register (Rev 1.6, p791), it states that when LCDEN is set to 0, then LCDLP, and LCDFP are set low. When I probe these lines, they are high in the disabled state.

I have these pins both considered with:
- pulldown enabled
- pullup disabled
- input buffer enabled
- glitch filter disabled
- FP/LP functions selected.

There's nothing in the errata about these pins resetting to an incorrect state. Is there more information I'm missing, or is this an error in the documentation or chip?
标签 (1)
0 项奖励
回复
0 回复数