Incorrect LCDFP and LCDLP states with LCDEN disabled.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Incorrect LCDFP and LCDLP states with LCDEN disabled.

638 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GregDavies on Wed Sep 16 08:35:44 MST 2015
In the user manual for the LCD Control register (Rev 1.6, p791), it states that when LCDEN is set to 0, then LCDLP, and LCDFP are set low. When I probe these lines, they are high in the disabled state.

I have these pins both considered with:
- pulldown enabled
- pullup disabled
- input buffer enabled
- glitch filter disabled
- FP/LP functions selected.

There's nothing in the errata about these pins resetting to an incorrect state. Is there more information I'm missing, or is this an error in the documentation or chip?
Labels (1)
0 Kudos
Reply
0 Replies