Incorrect LCDFP and LCDLP states with LCDEN disabled.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Incorrect LCDFP and LCDLP states with LCDEN disabled.

1,001件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GregDavies on Wed Sep 16 08:35:44 MST 2015
In the user manual for the LCD Control register (Rev 1.6, p791), it states that when LCDEN is set to 0, then LCDLP, and LCDFP are set low. When I probe these lines, they are high in the disabled state.

I have these pins both considered with:
- pulldown enabled
- pullup disabled
- input buffer enabled
- glitch filter disabled
- FP/LP functions selected.

There's nothing in the errata about these pins resetting to an incorrect state. Is there more information I'm missing, or is this an error in the documentation or chip?
ラベル(1)
0 件の賞賛
返信
0 返答(返信)