ISP over CAN - LPC11C24

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ISP over CAN - LPC11C24

1,724 次查看
trevorroach
Contributor I

Hello all,

I'm working on a project where we would ideally like to be able to flash a program via CAN ISP to an LPC11C24. The documentation provides fairly good guidelines on what to put on the CAN bus line in order to accomplish this, but I am somewhat lost as to how to get the binary file, etc from the PC to the CAN bus. We've considered creating a custom CAN programmer board, but would love to know if there is any NXP hardware/software already available for this purpose? 

If there are no NXP/third party solutions available, any further tips/advice would be much appreciated.

Thanks. 

标签 (3)
0 项奖励
回复
1 回复

1,228 次查看
soledad
NXP Employee
NXP Employee

Hi,

I'm afraid there are no such demos to meet your requirement.

However you can learn to form the CAN ISP sequence by checking the following link:

LPC11C24 Can Bootloader Assistance 

Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Like
0 项奖励
回复