Where Can I download the code of LPCOPEN-SOFTWARE-FOR-LPC546xx ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where Can I download the code of LPCOPEN-SOFTWARE-FOR-LPC546xx ?

860件の閲覧回数
songhanson
Contributor I

Where Can I download the code of  LPCOPEN-SOFTWARE-FOR-LPC546xx ?

以前可以从keil里下载到,现在也没有了。

还有,哪儿有LPCOpen的CAN FD的参考例程??

thanks

0 件の賞賛
返信
1 返信

759件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

There is no LPCOpen software for LPC546xx devices.

However you can use MCUXpresso SDK for these devices, you can download it from the next link:

Welcome to MCUXpresso | MCUXpresso Config Tools 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信