ISP over CAN - LPC11C24

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISP over CAN - LPC11C24

2,423件の閲覧回数
trevorroach
Contributor I

Hello all,

I'm working on a project where we would ideally like to be able to flash a program via CAN ISP to an LPC11C24. The documentation provides fairly good guidelines on what to put on the CAN bus line in order to accomplish this, but I am somewhat lost as to how to get the binary file, etc from the PC to the CAN bus. We've considered creating a custom CAN programmer board, but would love to know if there is any NXP hardware/software already available for this purpose? 

If there are no NXP/third party solutions available, any further tips/advice would be much appreciated.

Thanks. 

ラベル(3)
0 件の賞賛
返信
1 返信

1,927件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

I'm afraid there are no such demos to meet your requirement.

However you can learn to form the CAN ISP sequence by checking the following link:

LPC11C24 Can Bootloader Assistance 

Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Like
0 件の賞賛
返信