IAP sector0 issue on LPC54608

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IAP sector0 issue on LPC54608

1,552 Views
xiumei_li
NXP Employee
NXP Employee

Customer met sector0 program issue, and return “10221”, though it can be erased correctly. Other sectors also can be erased & programmed properly. Confirmed interrupt vectors reside is correct. Need to check the difference between sector0 and other sectors. 

Pls help assign this question to Alex Yang,he has got this issue by email. Thanks.

 

0 Kudos
Reply
1 Reply

1,525 Views
alex_yang
NXP Employee
NXP Employee

Hi, May,

 

This is probably caused by customer didn't add checksum value(VECTOR position and ROM API will check this checksum value and if the checksum wrong, it will return an error code.

see :

https://community.nxp.com/t5/LPC-Microcontrollers/IAP-sector0-issue-on-LPC54608/m-p/1321538#M46134

 

 

0 Kudos
Reply