IAP sector0 issue on LPC54608

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IAP sector0 issue on LPC54608

1,583件の閲覧回数
xiumei_li
NXP Employee
NXP Employee

Customer met sector0 program issue, and return “10221”, though it can be erased correctly. Other sectors also can be erased & programmed properly. Confirmed interrupt vectors reside is correct. Need to check the difference between sector0 and other sectors. 

Pls help assign this question to Alex Yang,he has got this issue by email. Thanks.

 

0 件の賞賛
返信
1 返信

1,556件の閲覧回数
alex_yang
NXP Employee
NXP Employee

Hi, May,

 

This is probably caused by customer didn't add checksum value(VECTOR position and ROM API will check this checksum value and if the checksum wrong, it will return an error code.

see :

https://community.nxp.com/t5/LPC-Microcontrollers/IAP-sector0-issue-on-LPC54608/m-p/1321538#M46134

 

 

0 件の賞賛
返信