I2S TX 4 pin mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2S TX 4 pin mode

1,350 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vdelabouere on Wed Oct 29 13:02:19 MST 2014
Hi,

I have the following I2S0 signals connections to a stereo CODEC.

I2S0_TX_MCLK connected to the CODEC
I2S0_TX_SCK connected to the CODEC
I2S0_TXWS connected to the CODEC
I2S0_TX_SDA connected to the DAC data input of the CODEC
I2S0_RX_SDA connected to the ADC data output of the CODEC

Because of this configuration, I decided to configure I2S0 transmitter as MASTER and I2S0 receiver in 4 wire mode (slave mode).
I then enable the RX interrupt for I2S0.

In this configuration I don't receive any RX interrupts !

Do you have any idea why ?
Is it some kind of limitation of the 4 wire mode ?

it doesn't really make any sense to me.

Thanks.

Vince


Labels (1)
0 Kudos
Reply
1 Reply

1,263 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vdelabouere on Thu Oct 30 11:39:39 MST 2014
Anyone has an idea for this problem ?

I cannot find any source code that uses this 4 pin mode.
I wonder if the user manual is missing something to properly activate this mode.

Thanks
Vince
0 Kudos
Reply