I2S TX 4 pin mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2S TX 4 pin mode

1,402件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vdelabouere on Wed Oct 29 13:02:19 MST 2014
Hi,

I have the following I2S0 signals connections to a stereo CODEC.

I2S0_TX_MCLK connected to the CODEC
I2S0_TX_SCK connected to the CODEC
I2S0_TXWS connected to the CODEC
I2S0_TX_SDA connected to the DAC data input of the CODEC
I2S0_RX_SDA connected to the ADC data output of the CODEC

Because of this configuration, I decided to configure I2S0 transmitter as MASTER and I2S0 receiver in 4 wire mode (slave mode).
I then enable the RX interrupt for I2S0.

In this configuration I don't receive any RX interrupts !

Do you have any idea why ?
Is it some kind of limitation of the 4 wire mode ?

it doesn't really make any sense to me.

Thanks.

Vince


ラベル(1)
0 件の賞賛
返信
1 返信

1,315件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vdelabouere on Thu Oct 30 11:39:39 MST 2014
Anyone has an idea for this problem ?

I cannot find any source code that uses this 4 pin mode.
I wonder if the user manual is missing something to properly activate this mode.

Thanks
Vince
0 件の賞賛
返信