I2C 5V Toterant

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,944件の閲覧回数
przemekmaslowsk
Contributor I

Good morning, I would like to ask if the "PIO0_4 / SCL" and "PIO0_5 / SDA" pins in I2C configuration of the microprocessor LPC1313FBD48/01 are 5V tolerant. Thanks so much

ラベル(1)
1 解決策
1,756件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

 Yes, they are 5 V tolerant.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,757件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

 Yes, they are 5 V tolerant.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------