I2C 5V Toterant

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C 5V Toterant

Jump to solution
1,943 Views
przemekmaslowsk
Contributor I

Good morning, I would like to ask if the "PIO0_4 / SCL" and "PIO0_5 / SDA" pins in I2C configuration of the microprocessor LPC1313FBD48/01 are 5V tolerant. Thanks so much

Labels (1)
1 Solution
1,755 Views
soledad
NXP Employee
NXP Employee

Hi,

 Yes, they are 5 V tolerant.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,756 Views
soledad
NXP Employee
NXP Employee

Hi,

 Yes, they are 5 V tolerant.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------