I am getting the following error when I do RUN->Debug.How can I get rid of this error. Error while launching command: arm-none-eabi-gdb --version

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I am getting the following error when I do RUN->Debug.How can I get rid of this error. Error while launching command: arm-none-eabi-gdb --version

4,367 次查看
mikijin
Contributor I

I am getting the following error  when I do RUN->Debug.How can I get rid of this error?

Message "Could not determine GDB version using command: arm-none-eabi-gdb --version"

But arm-none-eabi-gdb exists in C:\nxp\MCUXpressoIDE_10.2.0_759\ide\tools\bin. 

- Using device LPC1549

-Tool MCUXpresso 10.2.0_759

- probe Link Server LPC-LINK2 CMSIS-DAP V5.183



标签 (1)
0 项奖励
回复
5 回复数

4,188 次查看
mikijin
Contributor I

Thank you for the kindness reply. 

I use Windows 7. 

And my 2 bussiness PC doesn’t work. 

But the PC of my co-worker's and my home's with WIN7 PC could work well.  

So I think that would be due to PC, including that of environment.

I tried with the latest version of MCUXpresso 10.3.1_2233. but was not fixed. 

And I tried to reinstall many times but it was not fixed.

I will continue to analyze from various viewpoints. 

0 项奖励
回复

4,188 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mikimoto Jin,

Which system of your PC do you used?

Please check the Device Manager,  does it detect your Debug Probe.

And suggest you use the latest version of MCUXpresso IDEv10.3.1 :
MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP   

BR

Alice

0 项奖励
回复

4,188 次查看
mikijin
Contributor I

Sorry,

What I am saying is the same thing.
This is the phenomenon when you press the debug button.

and also same as Debug As "MCUXpresso IDE link server".

Regards,

0 项奖励
回复

4,188 次查看
converse
Senior Contributor V
0 项奖励
回复

4,188 次查看
converse
Senior Contributor V

Read the manual. It tells you to use the QuickStart Debug button, not the method you used.

0 项奖励
回复