I am getting the following error when I do RUN->Debug.How can I get rid of this error. Error while launching command: arm-none-eabi-gdb --version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I am getting the following error when I do RUN->Debug.How can I get rid of this error. Error while launching command: arm-none-eabi-gdb --version

4,369件の閲覧回数
mikijin
Contributor I

I am getting the following error  when I do RUN->Debug.How can I get rid of this error?

Message "Could not determine GDB version using command: arm-none-eabi-gdb --version"

But arm-none-eabi-gdb exists in C:\nxp\MCUXpressoIDE_10.2.0_759\ide\tools\bin. 

- Using device LPC1549

-Tool MCUXpresso 10.2.0_759

- probe Link Server LPC-LINK2 CMSIS-DAP V5.183



ラベル(1)
0 件の賞賛
返信
5 返答(返信)

4,190件の閲覧回数
mikijin
Contributor I

Thank you for the kindness reply. 

I use Windows 7. 

And my 2 bussiness PC doesn’t work. 

But the PC of my co-worker's and my home's with WIN7 PC could work well.  

So I think that would be due to PC, including that of environment.

I tried with the latest version of MCUXpresso 10.3.1_2233. but was not fixed. 

And I tried to reinstall many times but it was not fixed.

I will continue to analyze from various viewpoints. 

0 件の賞賛
返信

4,190件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mikimoto Jin,

Which system of your PC do you used?

Please check the Device Manager,  does it detect your Debug Probe.

And suggest you use the latest version of MCUXpresso IDEv10.3.1 :
MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP   

BR

Alice

0 件の賞賛
返信

4,190件の閲覧回数
mikijin
Contributor I

Sorry,

What I am saying is the same thing.
This is the phenomenon when you press the debug button.

and also same as Debug As "MCUXpresso IDE link server".

Regards,

0 件の賞賛
返信

4,190件の閲覧回数
converse
Senior Contributor V
0 件の賞賛
返信

4,190件の閲覧回数
converse
Senior Contributor V

Read the manual. It tells you to use the QuickStart Debug button, not the method you used.

0 件の賞賛
返信