How to reinvoke UART ISP mode on LPC1343

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to reinvoke UART ISP mode on LPC1343

3,509 Views
mikesimmonds
Contributor III

I want to simulate UART ISP on an Olimex Eval Board because the target hardware is not ready.

The target will use an LPC1313 and therefore ISP will be on the UART.

The Olimex Eval Board has an LPC1343 with the USB boot mode pin strapped high.

This cannot be changed.

So I wrote code to reinvoke ISP via the IAP command in the reset handler.

However, the part goes into USB mode ISP, and not UART.

How can I make the device enter UART ISP?

NB: The ISP checksum of my code is correct.

My Code:

    movs    r0, sRam        ; r0 --> 0x10000000
    adds    r1, r0, 0x20        ; r1 --> 0x10000020

    sub    sp, 32            ; set stack (IAP friendly)
    movs    r2, 57            ; IAP command: Reinvoke ISP
    str    r2, [r0]        ;

    ldr    r3, =0x1FFF1FF1        ; IAP entry point (thumb bit)
    bx    r3            ; IAP(r0, r1)

Cheers, Mike.

Labels (1)
0 Kudos
Reply
4 Replies

2,995 Views
mikesimmonds
Contributor III

Did you actually READ ALL of the original post? I know full well that the level on Port 0.3 selects between UART and USB mode,

THAT is the problem in a nutshell.

What [1] NXP engineer put the VBUS function on the same pin as the USB/UART pin-strap?

For a bus powered system it is IMPOSSIBLE to pull this pin to ground! That would short out the USB power pins

and, moreover would de-power the device so ANY boot function would fail. See the schematic attached.

Please, I would like a proper solution to invoking the UART ISP mode on a bus powered system with this device.

Perhaps, someone at NXP with access to the LPC1343 version 5.2 boot ROM source code could provide

an address to jump to that is after the test for port 0.3 low and will begin the UART mode ISP.

I really have not got either the time or the inclination to disassemble the boot ROM code myself.

[1] Insert you own adjective here.

Regards, Mike

0 Kudos
Reply

2,995 Views
renegeraets
NXP Employee
NXP Employee

In your schematic I see there is a 1k resistor (R9) between USB_VBUS and PIO0_3. This will limit the extra current drawn from VBus to 5 mA when you short P0_3 to gnd. That should not be a problem if you want to experiment with UART ISP.

Hope this helps

0 Kudos
Reply

2,995 Views
rolfmeeser
NXP Employee
NXP Employee

In addition to the valid solution which Rene suggested, there is also a software hack available.

You could use for your benefit what tons of people have done wrong by accident: Disconnect the digital input stage of the I/O pin! Right before calling the IAP_Reinvoke_ISP function, write 0x00000000 to the IOCON_PIO0_3 register. Then regardless of the actual voltage at the PIO0_3 pin, the boot code will always read it as 0, and should enter UART instead of USB mode.

0 Kudos
Reply

2,995 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

After execute the Reinvoke ISP command, the state of the PIO0_3 determines whether the UART or USB interface will be used.

2016-09-07_11-53-29.jpg
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply